Gets or sets the portion of the middle of a chirp region used for frequency and phase calculations in triangle-modulated pulses.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property PulseFrequencyPhaseRegionMeasurementWidth As Double |
| C# | |
|---|
public virtual double PulseFrequencyPhaseRegionMeasurementWidth {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double PulseFrequencyPhaseRegionMeasurementWidth {
double get();
void set ( double value);
} |
Property Value
The default value is 75%.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 20.00
See Also