Gets or sets the portion of the middle of a pulse used for Ripple calculation.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property PulseRippleMeasurementWidth As Double |
| C# | |
|---|
public abstract double PulseRippleMeasurementWidth {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double PulseRippleMeasurementWidth {
double get();
void set ( double value);
} |
Property Value
The default value is 50%.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 19.00
See Also