Keysight 89600 VSA .NET API
PulseWidthThreshold Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : PulseWidthThreshold Property


Glossary Item Box

Gets or sets the threshold for measuring pulse width.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PulseWidthThreshold As Double
C# 
public abstract double PulseWidthThreshold {get; set;}
C++/CLI 
public:
abstract property double PulseWidthThreshold {
   double get();
   void set (    double value);
}

Property Value

The default value is 50. The maximum is 100, and the minimum is 0%.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also