Gets or sets the upper threshold for measuring pulse rise time.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property RiseTimeUpperThreshold As Double |
| C# | |
|---|
public abstract double RiseTimeUpperThreshold {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double RiseTimeUpperThreshold {
double get();
void set ( double value);
} |
Property Value
The default value is 90
. The maximum is 100, and the minimum is 0%.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 19.00
See Also