| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub SavePulseDescriptorWordFile( _ ByVal filePath As String _ ) | |
Parameters
- filePath
- Absolute path plus file name
You can select whether to export just the results of the current measurement (in the Pulse Table) or export all pulses in the currently loaded recording using the PulseExportMode property.
When PulseExportMode = EntireRecording, the VSA will first play through the recording and collect the pulses, and then export the results to the PDW file.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.00