Keysight 89600 VSA .NET API
SaveScoringReferenceFile Method
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : SaveScoringReferenceFile Method


filePath
Absolute path plus file name

Glossary Item Box

Create a scoring reference file.

Syntax

Visual Basic (Declaration) 
Public Overridable Sub SaveScoringReferenceFile( _
   ByVal filePath As String _
) 
C# 
public virtual void SaveScoringReferenceFile( 
   string filePath
)
C++/CLI 
public:
virtual void SaveScoringReferenceFile( 
   String^ filePath
) 

Parameters

filePath
Absolute path plus file name

Remarks

Save current scoring reference to the file with Tab delimited text format that includes sequence of Top Level, Width, PRI, Frequency Mean and FM Slope. RecallScoringReferenceFile

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.20

See Also