Gets or sets the base error value of the Frequency Mean metric for scoring.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property ScoringFrequencyMeanBaseError As Double |
| C# | |
|---|
public virtual double ScoringFrequencyMeanBaseError {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double ScoringFrequencyMeanBaseError {
double get();
void set ( double value);
} |
Property Value
The default value is 10MHz.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 24.20
See Also