Keysight 89600 VSA .NET API
ScoringFrequencyMeanEnabled Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : ScoringFrequencyMeanEnabled Property


Glossary Item Box

Gets or sets a value indicating whether the Frequency Mean metric for scoring calculation is enabled.

Syntax

Visual Basic (Declaration) 
Public Overridable Property ScoringFrequencyMeanEnabled As Boolean
C# 
public virtual bool ScoringFrequencyMeanEnabled {get; set;}
C++/CLI 
public:
virtual property bool ScoringFrequencyMeanEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

Scoring for Frequency Mean enable/disable properties. If value is true, scoring includes the Frequency Mean metric.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.20

See Also