Keysight 89600 VSA .NET API
ScoringPriBaseError Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : ScoringPriBaseError Property


Glossary Item Box

Gets or sets the base error value of the PRI metric for scoring.

Syntax

Visual Basic (Declaration) 
Public Overridable Property ScoringPriBaseError As Double
C# 
public virtual double ScoringPriBaseError {get; set;}
C++/CLI 
public:
virtual property double ScoringPriBaseError {
   double get();
   void set (    double value);
}

Property Value

The default value is 100e-9 sec.

Remarks

Scoring is calculated based on the error of the PRI item.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.20

See Also