Keysight 89600 VSA .NET API
SegmentLength Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : SegmentLength Property


Glossary Item Box

Gets or sets the input signal segment length when doing segmented acquisition.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SegmentLength As Double
C# 
public abstract double SegmentLength {get; set;}
C++/CLI 
public:
abstract property double SegmentLength {
   double get();
   void set (    double value);
}

Property Value

The units are seconds. The default value is 10 µs.

Remarks

This is used only when segmented acquisition is enabled (when Time.IsSegmentedCapture is true).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also