Keysight 89600 VSA .NET API
SetAllModulationTypes Method
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : SetAllModulationTypes Method


enable
True enables all modulation types; false disables them

Glossary Item Box

Set or clear all modulation types that are detected

Syntax

Visual Basic (Declaration) 
Public Overridable Sub SetAllModulationTypes( _
   ByVal enable As Boolean _
) 
C# 
public virtual void SetAllModulationTypes( 
   bool enable
)
C++/CLI 
public:
virtual void SetAllModulationTypes( 
   bool enable
) 

Parameters

enable
True enables all modulation types; false disables them

Remarks

This applies to all properties of the type IsModulationTypeXXXEnabled.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.00

See Also