Keysight 89600 VSA .NET API
SetDeinterleaveMinAmplitudes Method
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : SetDeinterleaveMinAmplitudes Method


minAmplitudes
The array with four values indicating the min amplitudes for each emitter.

Glossary Item Box

Sets the minimum top level values for each emitter (dBm).

Syntax

Visual Basic (Declaration) 
Public Overridable Sub SetDeinterleaveMinAmplitudes( _
   ByVal minAmplitudes As IEnumerable(Of Single) _
) 
C# 
public virtual void SetDeinterleaveMinAmplitudes( 
   IEnumerable<float> minAmplitudes
)
C++/CLI 
public:
virtual void SetDeinterleaveMinAmplitudes( 
   IEnumerable<float>^ minAmplitudes
) 

Parameters

minAmplitudes
The array with four values indicating the min amplitudes for each emitter.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also