Keysight 89600 VSA .NET API
SidelobeKeepOutMode Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : SidelobeKeepOutMode Property


Glossary Item Box

Gets or sets the keep-out mode for time sidelobe calculations.

Syntax

Visual Basic (Declaration) 
Public Overridable Property SidelobeKeepOutMode As SidelobeKeepOutMode
C# 
public virtual SidelobeKeepOutMode SidelobeKeepOutMode {get; set;}
C++/CLI 
public:
virtual property SidelobeKeepOutMode SidelobeKeepOutMode {
   SidelobeKeepOutMode get();
   void set (    SidelobeKeepOutMode value);
}

Property Value

The default value is SidelobeKeepOutMode.FirstNull.

Remarks

This is ignored unless IsCorrelationEnabled is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20

See Also