Keysight 89600 VSA .NET API
PulseTimeStartReportMode Enumeration
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : PulseTimeStartReportMode Enumeration


Glossary Item Box

Specifies how time values are reported in traces and result tables.

Syntax

Visual Basic (Declaration) 
Public Enum PulseTimeStartReportMode 
   Inherits System.Enum
C# 
public enum PulseTimeStartReportMode : System.Enum 
C++/CLI 
public enum class PulseTimeStartReportMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
RelativeToFirstPulseTime values are reported relative to the first detected pulse's Rise Edge time.—
RelativeToTriggerTime values are reported relative to the trigger (or triggers for segmented acquisition).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also