Keysight 89600 VSA .NET API
TopBaseCalculationMethod Enumeration
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : TopBaseCalculationMethod Enumeration


Glossary Item Box

Methods for calculating the top and base levels of pulses.

Syntax

Visual Basic (Declaration) 
Public Enum TopBaseCalculationMethod 
   Inherits System.Enum
C# 
public enum TopBaseCalculationMethod : System.Enum 
C++/CLI 
public enum class TopBaseCalculationMethod : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
MeanThe mean (average level) is used to determine the top and base pulse levels.—
MedianThe median (50% of values are less than this, and 50% are greater) is used to determine the top and base pulse levels.—
ModeThe mode (most common value) is used to determine the top and base pulse levels.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also