Keysight 89600 VSA .NET API
TrainScoringCollection Class
Members  See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : TrainScoringCollection Class


Glossary Item Box

This class represents a collection of TrainScoring instances.

Object Model

TrainScoringCollection ClassTrainScoring ClassTrainBaseError ClassTrainReferencePulseCollection ClassTrainReferencePulse ClassTrainReferencePulse Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class TrainScoringCollection 
   Inherits Agilent.SA.Vsa.RemotableCollection(Of TrainScoring)
   Implements Agilent.SA.Vsa.ICollectionBase, Agilent.SA.Vsa.ICollectionBase(Of TrainScoring), Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyCollectionChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 

Remarks

The collection has a minimum length of 1 and maximum length of 16. The default count is 4.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also