Keysight 89600 VSA .NET API
TrainSearchModulationType Enumeration
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace : TrainSearchModulationType Enumeration


Glossary Item Box

Specifies the modulation type for train search scoring.

Syntax

Visual Basic (Declaration) 
Public Enum TrainSearchModulationType 
   Inherits System.Enum
C# 
public enum TrainSearchModulationType : System.Enum 
C++/CLI 
public enum class TrainSearchModulationType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BarkerPhaseThe pulse modulation is assumed to be BPSK with chips forming a Barker sequence.—
BpskThe pulse modulation is assumed to be BPSK.—
ContinuousWavePulse is assumed to be continuous wave (CW), i.e. not modulated.—
FrankCodeThe pulse modulation is assumed to be Frank Code.—
LinearFMThe pulse modulation is assumed to be linear frequency modulation (i.e. chirps).—
P1CodeThe pulse modulation is assumed to be P1 Code.—
P2CodeThe pulse modulation is assumed to be P2 Code.—
P3CodeThe pulse modulation is assumed to be P3 Code.—
P4CodeThe pulse modulation is assumed to be P4 Code.—
QpskThe pulse modulation is assumed to be QPSK.—
TriangularFMThe pulse modulation is assumed to be triangular FM.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also