Keysight 89600 VSA .NET API
AskPulseLowerThreshold Property
See Also 
Agilent.SA.Vsa.Rfid.Interfaces Assembly > Agilent.SA.Vsa.Rfid Namespace > MeasurementExtension Class : AskPulseLowerThreshold Property


Glossary Item Box

Gets or sets the ASK lower pulse threshold.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AskPulseLowerThreshold As Double
C# 
public abstract double AskPulseLowerThreshold {get; set;}
C++/CLI 
public:
abstract property double AskPulseLowerThreshold {
   double get();
   void set (    double value);
}

Remarks

Rise and fall times of ASK are determined by two threshold levels. The threshold levels are set in percent. ASK Meas Time trace is normalized so that On and Off amplitude levels become 100 and 0 respectively. Default value of the lower threshold level is 10%. This parameter is valid only in ASK measurement.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also