Keysight 89600 VSA .NET API
Agilent.SA.Vsa.Rfid Namespace
See Also  Inheritance Hierarchy
Agilent.SA.Vsa.Rfid.Interfaces Assembly : Agilent.SA.Vsa.Rfid Namespace

Glossary Item Box

The Agilent.SA.Vsa.Rfid namespace contains classes and enums to control  the RFID measurement features.

Classes

 ClassDescription
ClassMeasurementExtension The Rfid.MeasurementExtension object contains properties and members to control the RFID measurement features.

Enumerations

 EnumerationDescription
EnumerationDirectionType Specifies how to decode the examined portion of the RFID exchange.
EnumerationLineCodeType Specifies the forward and reverse line coding expected by the RFID demodulation software.
EnumerationMeasurementFilter Specifies the measurement filter.
EnumerationMeasurementMode Specifies the type of signal measurement.
EnumerationModulationFormat Specifies the modulation format of the RFID burst from the interrogator to the tag.
EnumerationReferenceFilter Specifies the reference filter.
EnumerationStandard Specifies a specific RFID protocol.
EnumerationStandardSynchronizationPattern Specifies the synch pattern from a set of standard protocol patterns.
EnumerationSynchronizationSearchType Specifies a bit pattern on which to sync the demodulation measurements.

See Also