| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property CWLowerThreshold As Double | |
| C# | |
|---|---|
public abstract double CWLowerThreshold {get; set;} | |
Rise and fall times of the Interrogator CW signal are determined by two threshold levels. These levels are specified as a percentage of the steady-state CW level. The default value of the lower threshold is 10%.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)