| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property ForwardTari As Double | |
| C# | |
|---|---|
public abstract double ForwardTari {get; set;} | |
The ForwardTari time (in seconds) is required when using PIE line encoding. The Tari value is specified by time because the bit rate varies depending on the data value encoded. ForwardTari is only used in PIE line encoding because the bit rate varies depending on the data pattern.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)