Keysight 89600 VSA .NET API
IsReturnLinkPassive Property
See Also 
Agilent.SA.Vsa.Rfid.Interfaces Assembly > Agilent.SA.Vsa.Rfid Namespace > MeasurementExtension Class : IsReturnLinkPassive Property


Glossary Item Box

Gets or sets a value indicating whether the return link is passive (true) or active (false).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsReturnLinkPassive As Boolean
C# 
public abstract bool IsReturnLinkPassive {get; set;}
C++/CLI 
public:
abstract property bool IsReturnLinkPassive {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also