| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IsSynchronizationSearchEnabled As Boolean | |
| C# | |
|---|---|
public abstract bool IsSynchronizationSearchEnabled {get; set;} | |
Setting this parameter to True allows you to measure a signal that has a certain symbol pattern. When the sync pattern is found, ResultOffset is set to [Head of sync pattern - Sync Offset] and the sync bit pattern is highlighted in the Demod Bits trace.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)