Keysight 89600 VSA .NET API
ResultLength Property
See Also 
Agilent.SA.Vsa.Rfid.Interfaces Assembly > Agilent.SA.Vsa.Rfid Namespace > MeasurementExtension Class : ResultLength Property


Glossary Item Box

Gets or sets the measurement start time interval in relation to acquisition time in seconds.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property ResultLength As Double
C# 
public abstract double ResultLength {get; set;}
C++/CLI 
public:
abstract property double ResultLength {
   double get();
   void set (    double value);
}

Remarks

This value is ignored when IsBurstSearchEnabled is on.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also