Keysight 89600 VSA .NET API
ReturnBitRate Property
See Also 
Agilent.SA.Vsa.Rfid.Interfaces Assembly > Agilent.SA.Vsa.Rfid Namespace > MeasurementExtension Class : ReturnBitRate Property


Glossary Item Box

Gets or sets the return (Tag -> Interrogator) bit rate in bits/second.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property ReturnBitRate As Double
C# 
public abstract double ReturnBitRate {get; set;}
C++/CLI 
public:
abstract property double ReturnBitRate {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also