Keysight 89600 VSA .NET API
MeasurementMode Enumeration
See Also 
Agilent.SA.Vsa.Rfid.Interfaces Assembly > Agilent.SA.Vsa.Rfid Namespace : MeasurementMode Enumeration


Glossary Item Box

Specifies the type of signal measurement.

Syntax

Visual Basic (Declaration) 
Public Enum MeasurementMode 
   Inherits System.Enum
C# 
public enum MeasurementMode : System.Enum 
C++/CLI 
public enum class MeasurementMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BothSpecifies both CW Analysis and Modulation Analysis modes and all results are computed.—
CWAnalysisSpecifies CW Analysis which measures the CW signal produced by the interrogator.—
ModulationAnalysisSpecifies Modulation Analysis which examines the modulation within the CW signal.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also