Keysight 89600 VSA .NET API
ModulationFormat Enumeration
See Also 
Agilent.SA.Vsa.Rfid.Interfaces Assembly > Agilent.SA.Vsa.Rfid Namespace : ModulationFormat Enumeration


Glossary Item Box

Specifies the modulation format of the RFID burst from the interrogator to the tag.

Syntax

Visual Basic (Declaration) 
Public Enum ModulationFormat 
   Inherits System.Enum
C# 
public enum ModulationFormat : System.Enum 
C++/CLI 
public enum class ModulationFormat : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AskDsbSpecifies a DSB-ASK format (Forward and Return).—
AskPRSpecifies a PR-ASK format (Forward).—
AskSsbSpecifies a SSB-ASK format (Forward).—
BpskAgilent Use Only.—
Fsk2Specifies a 2-FSK format (Forward and Return).—
OokSpecifies a OOK format (Forward and Return).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also