Keysight 89600 VSA .NET API
Standard Enumeration
See Also 
Agilent.SA.Vsa.Rfid.Interfaces Assembly > Agilent.SA.Vsa.Rfid Namespace : Standard Enumeration


Glossary Item Box

Specifies a specific RFID protocol.

Syntax

Visual Basic (Declaration) 
Public Enum Standard 
   Inherits System.Enum
C# 
public enum Standard : System.Enum 
C++/CLI 
public enum class Standard : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
EpcGlobalClass1Generation2Specifies EPC Global Class-1 Generation-2 UHF (ISO 18000-6 Type-C).—
Iso14443TypeASpecifies ISO 14443 Type-A.—
Iso14443TypeBSpecifies ISO 14443 Type-B.—
Iso15693Specifies ISO 15693.—
Iso180004Mode1Specifies ISO 18000-4 Mode-1.—
Iso180006TypeASpecifies ISO 18000-6 Type-A.—
Iso180006TypeBSpecifies ISO 18000-6 Type-B.—
Iso18092Specifies ISO 18092.—
NoneSpecifies no standard.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also