Keysight 89600 VSA .NET API
Remove Method
See Also 
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace > CarrierCollection Class : Remove Method


item
Carrier to remove from the collection

Glossary Item Box

Removes the indicated Carrier from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Remove( _
   ByVal item As Carrier _
) As Boolean
C# 
public abstract bool Remove( 
   Carrier item
)
C++/CLI 
public:
abstract bool Remove( 
   Carrier^ item
) 

Parameters

item
Carrier to remove from the collection

Return Value

True, if the Carrier was removed from the collection. False otherwise.

Remarks

The maximum number of Carrier items is 16, the minimum is 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also