| Class | Description | |
|---|---|---|
![]() | Carrier | Defines properties of a single Carrier for the ACP measurement |
![]() | CarrierCollection | This class represents a collection of carrier instances |
![]() | InterferingSignal | Defines properties for inter modulation testing. The specified inter modulation interference frequency range is excluded from the measurement when interference power present is turned on from Enabled. |
![]() | InterferingSignalCollection | This class represents a collection of InterferingSignal instances |
![]() | MeasurementExtension | This measurement extension performs a Adjacent Channel Power (ACP), which measures power levels of one or more modulated Carriers, and of spurious signal levels in specified frequency bands ("Offsets") relative to the carrier(s). The power levels in the Offsets are compared with PowerLimits specified in each Offset. The results report the power levels, whether they fail or pass the limit tests, and by how much. Limits can be specified in terms of absolute power or power relative to the power of a carrier or group of carriers. |
![]() | Offset | Defines properties of a frequency region where the ACP measurement is to be made. |
![]() | OffsetCollection | This class represents a collection of Offset instances |
![]() | PowerLimit | Defines power level limits for a particular Offset. |
![]() | PowerReference | Defines properties of a power reference used in calculating the ACP. |
![]() | QuickSetup | The AdjacentChannelPower.QuickSetup class contains properties and methods related to loading a user-defined measurement setup into a AdjacentChannelPower measurement extension. |
![]() | QuickSetupCollection | The AdjacentChannelPower.QuickSetupCollection class provides access to the QuickSetup objects available to a AdjacentChannelPower measurement extension. |
| Enumeration | Description | |
|---|---|---|
![]() | FailMask | Defines which limits are tested against |
![]() | MultibandMode | Specifies the mode to use when configuring multiband behavior. |
![]() | OffsetSide | Defines which side of a reference carrier the offset applies to in defining frequency regions. |
![]() | OffsetSpacing | Defines the points between which a frequency offset is measured. |
![]() | PowerReferenceSource | Specifies the method used to choose the power reference. |
![]() | ReferencePowerCalculation | Specifies the scaling of integrated power data, specifying either total power or power spectral density. |