Keysight 89600 VSA .NET API
MeasurementExtension Class
Members  See Also 
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace : MeasurementExtension Class


Glossary Item Box

This measurement extension performs a Adjacent Channel Power (ACP), which measures power levels of one or more modulated Carriers, and of spurious signal levels in specified frequency bands ("Offsets") relative to the carrier(s). The power levels in the Offsets are compared with PowerLimits specified in each Offset. The results report the power levels, whether they fail or pass the limit tests, and by how much. Limits can be specified in terms of absolute power or power relative to the power of a carrier or group of carriers.

Object Model

MeasurementExtension ClassCarrierCollection ClassCarrier ClassCarrier ClassMeasurementExtension ClassCarrierCollection ClassCarrier ClassCarrier ClassMeasurementExtension ClassCarrierCollection ClassMeasurementExtension ClassInterferingSignalCollection ClassOffsetCollection ClassPowerReference ClassQuickSetupCollection ClassInterferingSignalCollection ClassInterferingSignal ClassInterferingSignal ClassOffsetCollection ClassOffset ClassOffset ClassPowerReference ClassQuickSetupCollection ClassQuickSetup ClassInterferingSignalCollection ClassInterferingSignal ClassInterferingSignal ClassOffsetCollection ClassOffset ClassPowerLimit ClassOffset ClassPowerLimit ClassPowerReference ClassQuickSetupCollection ClassQuickSetup Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class MeasurementExtension 
   Inherits Agilent.SA.Vsa.MeasurementExtension
   Implements Agilent.SA.Vsa.IMeasurementExtension, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IMeasurementBase, Agilent.SA.VsaInternal.IMeasurementBase2, Agilent.SA.VsaInternal.IMeasurementBase3, Agilent.SA.VsaInternal.IMeasurementBase4, Agilent.SA.VsaInternal.IMeasurementBase5, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 
C# 
public abstract class MeasurementExtension : Agilent.SA.Vsa.MeasurementExtension, Agilent.SA.Vsa.IMeasurementExtension, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IMeasurementBase, Agilent.SA.VsaInternal.IMeasurementBase2, Agilent.SA.VsaInternal.IMeasurementBase3, Agilent.SA.VsaInternal.IMeasurementBase4, Agilent.SA.VsaInternal.IMeasurementBase5, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  
C++/CLI 
public ref class MeasurementExtension abstract : public Agilent.SA.Vsa.MeasurementExtension, Agilent.SA.Vsa.IMeasurementExtension, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IMeasurementBase, Agilent.SA.VsaInternal.IMeasurementBase2, Agilent.SA.VsaInternal.IMeasurementBase3, Agilent.SA.VsaInternal.IMeasurementBase4, Agilent.SA.VsaInternal.IMeasurementBase5, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.20

See Also