| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function Remove( _ ByVal item As Offset _ ) As Boolean | |
Parameters
- item
- Offset to remove from the collection
Return Value
True, if the Offset was removed from the collection. False otherwise.The maximum number of Offset items is 16, the minimum is 1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)