Keysight 89600 VSA .NET API
OffsetSide Enumeration
See Also 
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace : OffsetSide Enumeration


Glossary Item Box

Defines which side of a reference carrier the offset applies to in defining frequency regions.

Syntax

Visual Basic (Declaration) 
Public Enum OffsetSide 
   Inherits System.Enum
C# 
public enum OffsetSide : System.Enum 
C++/CLI 
public enum class OffsetSide : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BothTwo frequency regions are defined, one above and one below the reference carrier.—
LowerFrequency region is below the reference carrier.—
UpperFrequency region is above the reference carrier.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.20

See Also