Keysight 89600 VSA .NET API
FailMask Property
See Also 
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace > PowerLimit Class : FailMask Property


Glossary Item Box

Gets or sets what types of failures are reported.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FailMask As FailMask
C# 
public abstract FailMask FailMask {get; set;}
C++/CLI 
public:
abstract property FailMask FailMask {
   FailMask get();
   void set (    FailMask value);
}

Property Value

The default value is FailMask.Relative.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also