Keysight 89600 VSA .NET API
Psd Property
See Also 
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace > PowerReference Class : Psd Property


Glossary Item Box

Gets or sets the PSD power (in dBm/Hz) used for the power reference.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Psd As Double
C# 
public abstract double Psd {get; set;}
C++/CLI 
public:
abstract property double Psd {
   double get();
   void set (    double value);
}

Property Value

The default value is 0.0 dBm/Hz.

Remarks

This value is used when PowerReferenceSource.Manual and ReferencePowerCalculation.Psd are specified.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also