Keysight 89600 VSA .NET API
QuickSetupCollection Class
Members  See Also 
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace : QuickSetupCollection Class


Glossary Item Box

The AdjacentChannelPower.QuickSetupCollection class provides access to the QuickSetup objects available to a AdjacentChannelPower measurement extension.

Object Model

QuickSetupCollection ClassQuickSetup Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class QuickSetupCollection 
   Inherits Agilent.SA.Vsa.RemotableCollection(Of QuickSetup)
   Implements Agilent.SA.Vsa.ICollectionBase, Agilent.SA.Vsa.ICollectionBase(Of QuickSetup), Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyCollectionChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 

Remarks

QuickSetups cannot be created or removed programmatically. The create and remove operations must take place through the GUI.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.20

See Also