Keysight 89600 VSA .NET API
AdaptiveEqualizerMode Enumeration
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace : AdaptiveEqualizerMode Enumeration


Glossary Item Box

Determines which impairments are tracked.

Syntax

Visual Basic (Declaration) 
Public Enum AdaptiveEqualizerMode 
   Inherits System.Enum
C# 
public enum AdaptiveEqualizerMode : System.Enum 
C++/CLI 
public enum class AdaptiveEqualizerMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
HoldTrackWithXCorrelation: the equalization impulse response is hold on last equalization impulse response.
OffOff: there is no tracking for equalization impulse response, so the equalization impulse response is re-calculated for each run. In ConfigurationModeSelection.Basic MeasurementExtension.ConfigurationMode, the equalizer is completely disabled.
TrackTrack: the equalization impulse response is updated run by run.
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also