Keysight 89600 VSA .NET API
Keysight.SA.Vsa.FlexFrame Namespace
See Also  Inheritance Hierarchy
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly : Keysight.SA.Vsa.FlexFrame Namespace

Glossary Item Box

Classes

 ClassDescription
ClassAllocation Settings to define an allocation.
ClassAllocationCollection This class represents a collection of allocations in a FrameDefinition.
ClassCarrierAggregation Settings for carrier aggregation.
ClassComponentCarrier Settings for a component carrier.
ClassComponentCarrierCollection This class represents a collection of component carrier instances.
ClassCustomModulation This class represents a modulation with custom symbol and IQ pairs.
ClassCustomModulationCollection This class represents a collection of imported custom modulations.
ClassCustomModulationState This class is for setting parameters for individual states within a custom modulation defined for use in Flex Frame modulation analysis.
ClassFrameDefinition Settings for defining a frame and its allocations.
ClassFramePart A class used to group allocations for measurement result reporting purposes.
ClassFramePartCollection Represents a collection of FrameParts.
ClassMeasurementExtension Settings for the FlexFrame measurement.
ClassQuickSetup The QuickSetup class contains properties and methods related to loading a user-defined measurement setup into a FlexFrame measurement extension.
ClassQuickSetupCollection The QuickSetupCollection class provides access to the QuickSetups available to a FlexFrame measurement extension.
ClassScrambler Provides settings to configure scramblers to be used by the Allocations in a FrameDefinition.
ClassScramblerCollection Represents a collection of Scramblers.
ClassScramblingConfiguration Provides settings for configuring scrambling for a ComponentCarrier.
ClassSingleCarrier Simplified API for single carrier measurements. Use CarrierAggregation for multi-carrier measurements or to access the full set of features available in the FlexFrame measurement.
ClassWaveformGeneration Settings for WaveformGeneration.

Enumerations

 EnumerationDescription
EnumerationAdaptiveEqualizerMode Determines which impairments are tracked.
EnumerationAllocationType Type of allocation.
EnumerationBitToSymbolMappingType Specifies the type of constellation bit mapping to be used.
EnumerationConfigurationModeSelection Specifies the configuration mode of the FlexFrame API.
EnumerationCustomModulationConstellation Constellation type used in custom modulation.
EnumerationCustomModulationConstellationStyle Presets for use as a starting point in creating a constellation definition.
EnumerationCustomSequenceStyle Type of custom sequence for allocations with Allocation.PayloadType = PayloadType.Custom.
EnumerationDvbModulationCoding Defines the constellation/bit mapping for DVB-S2/S2X when Allocation.Modulation=ModulationFormat.DvbS2S2xApsk.
EnumerationEqualizationMode Determines which mode to use when computing the equalizing filter.
EnumerationEqualizationOptimizationMode Specifies the type of the optimizer used in the LMS equalizer.
EnumerationEqualizationSource Determines which allocations are used to determine the channel estimate used to equalize the frame.
EnumerationFilterType Measurement or Reference Filter type.
EnumerationFrameDefinitionStyle Type of frame (bursted or periodic).
EnumerationFrequencyEstimationMode Determines the mode of frequency error estimation and compensation.
EnumerationModulationFormat Allocation modulation format.
EnumerationPayloadType Type of payload contained by an allocation.
EnumerationPhaseTrackingInterpolationMode Determines the interpolation mode for phase tracking.
EnumerationPhaseTrackingMode Determines the mode of phase tracking.
EnumerationReferenceFrequencyDefinition Reference Frequency Definition.
EnumerationSequenceType Specifies the type of scrambling to perform.
EnumerationStandard Available standard presets.
EnumerationSynchronizationMode Determines which allocations are used for initial synchronization.
EnumerationWaveformPredistortionMode WaveformPredistortionMode.

See Also