Keysight 89600 VSA .NET API
IncludedInEvm Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > Allocation Class : IncludedInEvm Property


Glossary Item Box

Gets or sets a value indicating whether the frame segment is included in overall EVM calculation.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IncludedInEvm As Boolean
C# 
public abstract bool IncludedInEvm {get; set;}
C++/CLI 
public:
abstract property bool IncludedInEvm {
   bool get();
   void set (    bool value);
}

Remarks

Not applicable for AllocationType.Idle segments.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also