Keysight 89600 VSA .NET API
SetBitSequence Method
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > Allocation Class : SetBitSequence Method


bitValues
array of integers where each integer is 0 or 1, representing a binary bit

Glossary Item Box

Sets the bit sequence used when CustomSequenceStyle = CustomSequenceStyle.BitSequence and PayloadType = PayloadType.Custom.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub SetBitSequence( _
   ByVal bitValues() As Integer _
) 
C# 
public abstract void SetBitSequence( 
   int[] bitValues
)
C++/CLI 
public:
abstract void SetBitSequence( 
   array<int>^ bitValues
) 

Parameters

bitValues
array of integers where each integer is 0 or 1, representing a binary bit

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also