Gets or sets the index of the carrier shown in Demod traces that are not fixed to a specific
ComponentCarrier.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property DisplayedCarrierIndex As Integer |
| C# | |
|---|
public virtual int DisplayedCarrierIndex {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int DisplayedCarrierIndex {
int get();
void set ( int value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 26.00
See Also