Keysight 89600 VSA .NET API
FilterAlpha Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > CarrierAggregation Class : FilterAlpha Property


Glossary Item Box

Gets or sets the ComponentCarrier.FilterAlpha for the carriers. The getter gets the value from the first carrier and the setter sets the value for all carriers.

Syntax

Visual Basic (Declaration) 
Public Overridable Property FilterAlpha As Double
C# 
public virtual double FilterAlpha {get; set;}
C++/CLI 
public:
virtual property double FilterAlpha {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00

See Also