Gets or sets a value indicating whether to compensate the signal for measured IQ imbalance for the carriers. See
ComponentCarrier.IQImbalanceCompensationEnabled. The getter gets the value from the first carrier and the setter sets the value for all carriers.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property IQImbalanceCompensationEnabled As Boolean |
| C# | |
|---|
public virtual bool IQImbalanceCompensationEnabled {get; set;} |
| C++/CLI | |
|---|
public:
virtual property bool IQImbalanceCompensationEnabled {
bool get();
void set ( bool value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 26.00
See Also