Keysight 89600 VSA .NET API
IQOffsetCompensationEnabled Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > CarrierAggregation Class : IQOffsetCompensationEnabled Property


Glossary Item Box

Gets or sets a value indicating whether to compensate the signal for measured IQ offset for the carriers. See ComponentCarrier.IQOffsetCompensationEnabled. The getter gets the value from the first carrier and the setter sets the value for all carriers.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IQOffsetCompensationEnabled As Boolean
C# 
public virtual bool IQOffsetCompensationEnabled {get; set;}
C++/CLI 
public:
virtual property bool IQOffsetCompensationEnabled {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00

See Also