Gets or sets the frame
FrameDefinition.Length for the carriers in symbols. The getter gets the value from the first carrier and the setter sets the value for all carriers.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property Length As Integer |
| C# | |
|---|
public virtual int Length {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int Length {
int get();
void set ( int value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 26.00
See Also