Keysight 89600 VSA .NET API
ResultLength Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > CarrierAggregation Class : ResultLength Property


Glossary Item Box

Gets or sets the ResultLength for the carriers in symbols. The getter gets the value from the first carrier and the setter sets the value for all carriers.

Syntax

Visual Basic (Declaration) 
Public Overridable Property ResultLength As Integer
C# 
public virtual int ResultLength {get; set;}
C++/CLI 
public:
virtual property int ResultLength {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00

See Also