Keysight 89600 VSA .NET API
Remove Method
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > ComponentCarrierCollection Class : Remove Method


item
ComponentCarrier to remove from the collection

Glossary Item Box

Removes the indicated ComponentCarrier from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Remove( _
   ByVal item As ComponentCarrier _
) As Boolean
C# 
public abstract bool Remove( 
   ComponentCarrier item
)
C++/CLI 
public:
abstract bool Remove( 
   ComponentCarrier^ item
) 

Parameters

item
ComponentCarrier to remove from the collection

Return Value

True, if the ComponentCarrier was removed from the collection. False otherwise.

Remarks

The maximum and minimum number of ComponentCarrier items is 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also