| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function Remove( _ ByVal item As CustomModulation _ ) As Boolean | |
| C# | |
|---|---|
public abstract bool Remove( CustomModulation item ) | |
| C++/CLI | |
|---|---|
public: abstract bool Remove( CustomModulation^ item ) | |
Parameters
- item
- CustomModulation to remove from the collection
Return Value
True, if the CustomModulation was removed from the collection. False otherwise.The minimum number of CustomModulation items is 1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)