Keysight 89600 VSA .NET API
RemoveAt Method
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > CustomModulationCollection Class : RemoveAt Method


index
Zero-based index of user to remove from the collection

Glossary Item Box

Removes the CustomModulation at the indicated index from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function RemoveAt( _
   ByVal index As Integer _
) As Boolean
C# 
public abstract bool RemoveAt( 
   int index
)
C++/CLI 
public:
abstract bool RemoveAt( 
   int index
) 

Parameters

index
Zero-based index of user to remove from the collection

Return Value

True, if the CustomModulation was removed from the collection. False otherwise.

Remarks

The minimum number of CustomModulation items is 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also