Keysight 89600 VSA .NET API
CustomModulationConstellation Enumeration
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace : CustomModulationConstellation Enumeration


Glossary Item Box

Constellation type used in custom modulation.

Syntax

Visual Basic (Declaration) 
Public Enum CustomModulationConstellation 
   Inherits System.Enum
C# 
public enum CustomModulationConstellation : System.Enum 
C++/CLI 
public enum class CustomModulationConstellation : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BpskBPSK modulation
Psk88-PSK modulation
Qam10241024-QAM modulation
Qam1616-QAM modulation
Qam256256-QAM modulation
Qam6464-QAM modulation
QpskQPSK modulation
UserDefinedUser Defined29.40
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.40

See Also